Page top

Primary Contents

Question

What is a manual reset?

Answer



A manual reset is a selectable feature of the interlock function.

When the Safety Sensor enters the interlock state, it keeps the control outputs in the OFF state. Even if all beams become free, the control outputs will not go to the ON state.

When none of the beams are interrupted in the detection zone and it is safe to operate the device, applying the reset input will reset the interlock condition and the control outputs will go to the ON state.

Applicable models:

F3SN Series Safety Light Curtain

F3SH Series Multi Beam Safety Sensor

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Sensors FAQ