Page top

Lead Contents

FAQ00176 of Programmable Terminals FAQ

FAQ No. FAQ00176

Primary Contents


What is the baud rate of high-speed 1:N NT Link communications? Also, how can I switch communications from the standard NT Link protocol?


The high-speed NT Link's baud rate is 115 kbps.

To set the high-speed NT Link, select the 1:N NT Link protocol in the Programmable Controller Setup and set the baud rate to 115 kbps.

Communications must be set to high-speed 1:N NT Link in the Programmable Terminal as well. Set the communications method in the Programmable Terminal's System Menu.