Page top

Primary Contents

Question

What is the difference between methods to use a terminating resistor attached to the T-branch Tap or a Terminal Block style terminating resistor of the DeviceNet?

Answer



It differs by whether the T-branch Tap "DCN1-1C" and/or "DCN1-3C" is located within 6m or more than 6m far from a node of the main line.

If it is located within 6m from a node of the main line, a supplied terminating resistor can be attached to the T-branch Tap.

If it is located more than 6m far from a node of the main line, a terminating resistor must be attached to the end of the node.

In this case, the T-branch Tap fitted with a terminating resistor or the Terminal Block style terminating resistor DRST-1 must be connected. The maximum cable length between the node and the terminating resistor is 1m.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Field Networks FAQ