Page top

Primary Contents

Question

Can the Flange Antennas and Flat Diversity Antennas used with the WM30 Wireless Modem be used with WD30 DeviceNet Wireless Units?

Answer



The Flange Antennas and Flat Diversity Antennas for the WM30 are designed for the WM30, and so they cannot be used with the WD30.

Use the Antennas that are supplied with the WD30. The following table lists the Antennas supplied with each model.

ModelSupplied Antenna
WD30-MEPencil Antenna
WD30-SEPencil Antenna
WD30-ME01Magnet-base Antenna
WD30-SE01Magnet-base Antenna

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Field Networks FAQ