![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Which Basic Switches are suitable as door switches?
Answer
Hinge roller models are suitable.
Example: Z-GW22 Basic Switch
Sliding Door 1:
Note:Push the actuator to approximately 70% to 100% of standard OT.
Note:When the door is closed, the slant of the dog is the first place that the actuator roller contacts.
Sliding Door 2:
D-type, Q-type, and S-type Pushbutton Models can also be used for the actuator.
Note:Push the actuator to approximately 70% to 100% of the standard OT.
Double Door:
D-type, Q-type, and S-type Pushbutton Models can also be used for the actuator.
Note:Push the actuator to approximately 70% to 100% of the standard OT.
Closet:
Note:The dog concept is the same as in Sliding Door 1, above.