Page top

Primary Contents

Question

What is snap-action?

Answer



Snap action is a mechanism that enables a movable contact to quickly travel from one fixed contact to another fixed contact regardless of the speed at which the Switch is operated.

The high switching speed shortens the time arcing is maintained.

Contact wear and damage are reduced, so stable characteristics can be obtained.

Large-capacity switching can be performed with compact models.

Recommended Products

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL / WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

D4A-[]N

The Limit Switch with Better Seal, Shock Resistance, and Strength

Other Basic Switches FAQ