![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Are there any Basic Switches or Limit Switches that can be used at high or low temperatures?
Answer
Yes, the models in the following table can be used at high or low temperatures. However, not all models are necessarily available even though the model number legends give them.
Heat-resistant Limit Switches and Basic Switches
| Switch type | Model | Heat resistance |
| Limit Switch | WL[]-TH | 5 to 120°C |
| Limit Switch | VE[]-TH | 5 to 100°C |
| Basic Switch | TZ | -65 to 400°C |
| Basic Switch | V[]-T | -25 to 150°C |
Cold-resistant Limit Switches and Basic Switches
| Switch type | Model | Cold resistance |
| Limit Switch | D4C-[]-C | -40 to 70°C |
| Limit Switch | D4CC-[]-C | -40 to 70°C |
| Limit Switch | WL[]-TC | -40 to 40°C |
| Limit Switch | D4A-[]N-T | -40 to 100°C |
| Limit Switch | SHL-[]-TC | -40 to 70°C |
| Limit Switch | VE-[]-TC | -40 to 70°C |
| Limit Switch | ZE/XE-[]TC | -20 to 50°C |
| Limit Switch | ZV/XV-[]TC | -20 to 50°C |
| Limit Switch | ZV2/XV2-[]TC | -20 to 50°C |
| Limit Switch | Z-[]-TC | -25 to 80°C |