Page top

Primary Contents

Question

Can the camera cable for the F500 Vision Sensor be extended?

Answer



The digital camera cable can be extended up to 10 m.

The standard length of a F500-VS Cable is 2 m, but 5-m and 10-m cables are also available.

To place an order, specify the desired length after the model number. (e.g., F500-VS 5M or F500-VS 10M)

The F500-VS Camera Cable includes the F500-VSD Camera Link Cable and the F500-VSP Camera Power Cable as a set.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Vision Sensors FAQ