Page top

Primary Contents

Question

Console cables for Vision Sensors can be extended?

Answer



Standard cable length of the Console "F150-KP" is 2m. Other than this, however, cables of 5m and 10m length are also available.
When ordering, specify the cable length with the model name: F150-KP 5M or F150-KP 10M.
Console "F160-KP" is only available in length of 2m. This is because the console incorporates the IC which can not operate when voltage drop occurs due to the cable extension.
Therefore, it is recommended that the F160-KP should be used with standard length.

Recommended Products

E2E

Standard Sensors for Detecting Ferrous Metals under Standard Conditions

E32 Series

OMRON's Fiber Sensors continue to support an increasing range of applications.

FZ2 Series

Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.

Other Vision Sensors FAQ