Page top

Primary Contents

Question

Can the actuator of WL Limit Switch be mounted on other Limit Switches?

Answer



Lever actuators can be mounted on the following models.

Applicable models: HL Limit Switch, D4C Limit Switch, D4CC Limit Switch, D4AN Limit Switch

Note:The roller weight will increase when a large the WL lever roller or long lever is used.

Mounting these types of levers on the HL, D4C, or D4CC may result in reset failure. Use the Limit Switch with the lever mounted downward.

Recommended Products

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL / WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

D4A-[]N

The Limit Switch with Better Seal, Shock Resistance, and Strength

Other Limit Switches FAQ