Page top

Lead Contents

FAQ02351 of Safety Limit Switches FAQ

FAQ No. FAQ02351

Primary Contents


What is a snap action?


SPST-NC + SPST-NO Contact (Snap Action) Example

The SPST-NC + SPST-NO contact snap action switches have the direct opening mechanism (forcibly opened contacts) defined under EN 60497-5-1. The NC contact side is the only side with a direct opening mechanism (forcibly opened contacts).

1. When contact welding occurs.

2. When contacts are being pulled apart.

Safety cam directly pushes up the movable contact blade.

3. When contacts are completely pulled apart.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Limit Switches FAQ