Page top

Lead Contents

FAQ02355 of Safety Limit Switches FAQ

FAQ No. FAQ02355

Primary Contents

Question

What is a direct opening mechanism (forcibly opened contacts) ?

Answer



A direct opening mechanism is one that forces open a welded contact by the direct force applied by the actuator (operating section) pressing down.
Safety components with direct opening mechanism (forcibly opened contacts) display the mark(*) on their labels.

Direct Opening Mechanism (Forcibly Opened Contacts)

After the contacts have been forced open, the contacts have enough insulation between them to clear the stipulated impulse withstand voltage (EN 60947-5-1) when the specified operating force (corresponding to DOF) or stroke (corresponding to DOT) is applied against a force of 10 N applied to the contacts (equivalent to the contact weld force).

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Limit Switches FAQ