Page top

Lead Contents

FAQ02381 of Safety Limit Switches FAQ

FAQ No. FAQ02381

Primary Contents


What is the conduit section?


The duct openings and wiring openings in Safety Door Switches and Safety Limit Switches are called the conduit sections and this is where the wiring section is sealed.
Refer to the following photographs of structural cross-sections of a D4BS-series Switch.

In the conduit size column in the catalogs, Pg13.5 and M20 are European specifications, G1/2 is the Japanese specification, and 1/2-14NPT is the North American specification.

Example:The conduit section and sizes for the conduit section for D4BS Safety Door Switches are shown below.

Difference between One-conduit, Two-conduit, and Three-conduit Models

One-conduit models have one conduit section on the switch.

Two-conduit models have two conduit sections on the switch

Three-conduit models have three conduit sections on the switch.

One-conduit Model

Example: D4DS-15FS

Two-conduit Model

Example: D4DS-55FS

Three-conduit Model

Example: D4BS-55FS

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Limit Switches FAQ