![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the cause of the E23 error in an R88D-HT10 Servo Driver?
Answer
The 23 error occurs when there is an open phase in the main circuit. An error is detected when a low voltage was detected in the main circuit's input section and lasted longer than 50 ms.
The likely causes of the error are that the main voltage power supply is not being input or there is an open phase in the main circuit. In general, this error is caused by a problem to the power supply input section. Check the main circuit power supply wiring.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.