![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What kind of noise is generated when the Servo System is used? Also what kind of noise affects the operation of the Servo System?
Answer
1. What Is Noise?
Noise is an unexpected random signal. Some noise originates from natural phenomena, such as lightening, but most noise that actually affects the operation of a device is created artificially inside or external to the device. Think of noise as an artificially created signal that travels through a transmission path to another signal line.
2. Types of Noises
Noise Sources
Devices that cause rapid changes in voltage or current are noise sources.
The more rapid the changes, the higher the voltage, and the higher the current, the stronger the noise source becomes.
| Coil surge | An electrical surge is generated when the voltage applied to the coil is switched ON/OFF. | Relay Solenoid Contactor | ![]() |
| Capacitor charge current | When voltage is applied to the capacitor it causes a large charge current flow. | Internal power source Power source Discharge device | ![]() |
| Pulse voltage | Pulse voltage from PWM (See note.) | Servo Driver Inverter Switching power | ![]() |
| Arc discharge | Rapid change in voltage when there is discharge | Welding machine Discharge tube | ![]() |
Note:PWM (pulse width modulation) is a method used to alter the voltage. By switching the voltage ON/OFF at a fast switching frequency, the average voltage can be modified.
3. Transmission Path of Noise
There are the following four noise transmission paths.
(1) Electrostatic Coupling Line
Signals that change rapidly are transmitted through a capacitor between other signal lines that cannot be seen (an electrical field). The more rapid the signal change, and the closer the signal line, the easier it is to transmit the signal.
Effects
Noise transmission between signal cables
Leakage current of the motor
Malfunction of Sensors in mechanical system
(2) Conductive Coupling Line
Signals that change rapidly are transmitted through a conductor (such as cables and frame grounds (FG)) to signal lines and control devices.
Noise may be transmitted through the power lines, or pass through other noise transmission paths before being transmitted by conduction.
Effects
Malfunction of control devices
Noise from power system
(3) Electromagnetic Induction Line
Signals that change rapidly create magnetic fields that change rapidly in the surrounding. A magnetic field generates electromotive force in other signal lines. The more rapid the signal changes, and the closer the signal line, the larger the electromotive force.
Effects
Noise transmission between signal cables
Noise from the motor power lines
(4) Electromagnetic Wave Line
Signals that change rapidly create magnetic waves that are emitted using the signal lines as antennas. In a Servo System, noise may be come from the sections shown in the diagram on the right.
Effects
Noise from radio or television
Malfunction of Sensors that use electromagnetic waves
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.