![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Please tell me of any precautions for extending the lead wires of a Temperature Sensor.
Answer
Platinum-resistance Thermometers
All three lead wires used for extension must have the same resistance and the same length. The extension will cause the resistance of the lead wires to affect the display temperature, so use lead wires with thick conductors. (OMRON does not carry lead wires for extension. Use commercially available lead wires.)
Thermocouples
Be sure to use compensating conductors for the extension. Also, select compensating conductors that suit the characteristics of the Thermocouple. Do not extend the lead wires with compensating conductors that do not suit the characteristics of the Thermocouple, or with ordinary lead wires, as this would prevent proper temperature measurement. Be sure also to connect the wires using the correct polarity (+/-).
Thermistors
Use lead wires with thick conductors for extension. There is no polarity.
General Precautions
Be careful of the cable routing because extending the lead wires makes the Sensor more susceptible to the effects of electrical noise.
Applicable Models: All models
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer