Page top

Primary Contents

Question

How do I change the displayed temperature if the displayed temperature is different from the actual temperature on the E5CS?

Answer



Use the input shift. The setting method is given below.

E5CS

1. Setting Input Shift

If the SP falls outside the temperature range when the temperature range is changed, the SP will be displayed first. The SP will be changed automatically either to the minimum value or the maximum value, whichever is nearest.

If the alarm value falls outside the temperature range when the temperature range is changed, the alarm value will be displayed first. The alarm value will be changed automatically to the maximum value in the new temperature range.

2. Operation Type Setting

Use the control mode switches to change the control mode. (All switches are OFF for the default settings.)

Function selection123456
ON/OFF PIDPID controlON
ON/OFF controlOFF
Control period2 sON
20 sOFF
Direct/reverse
operation
Direct operation (cooling)ON
Reverse operation (heating)OFF
Input shift
display
EnabledON
DisabledOFF
Temperature
Sensor
selection
ThermocoupleK, LON
K, JOFF
Platinum resistance
thermometer
Pt100ON
JPt100OFF
Multi-input
(thermocouple/platinum
resistance thermometer)
Platinum resistance
thermometer input
ON
Thermocouple inputOFF
Temperature
unit
°FON
°COFF

Note:The previous name Pt100 has been changed to JPt100 in accordance with revisions to JIS. The previous name J-DIN has been changed to L in accordance with revisions to DIN standards.

Turn ON switch 4, and after turning ON the power, press the Mode Key until H0 (indicates input shift of 0) is displayed. Press the Up and Down Keys to set the shift value.

Input shift displayMeasured temperatureTemperature display
H0 (no shift)100°C100°C
H9 (+9°C shift)100°C109°C
L9 (-9°C shift)100°C91°C

Note:When control mode switch 4 is turned OFF (no input shift display), the input shift is not displayed but the shift value is enabled. To disable input shift, set the input shift value to h0. The shift range depends on the setting unit.

Setting unit1°C0.1°C
Compensation range-99 to +99°C-9.9 to +9.9°C
Input shift displayL99 to H99L9.9 to H9.9

Applicable Models: E5CS

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Temperature Controllers FAQ