Page top

Primary Contents

Question

What's the difference between a Pt100 and JPt100 resistance thermometer?

Answer



In January 1, 1989, the JIS standard for platinum resistance thermometers (Pt100) was revised to incorporate the IEC (International Electrotechnical Commission) standard. The new JIS standard was established on April 1, 1989. Platinum resistance thermometers prior to the JIS standard revision are distinguished as JPt100. Therefore, make sure that the correct resistance thermometer - Glossary of Industrial Automation">platinum resistance thermometer is being used.

The following table shows the differences in appearance of the Pt100 and JPt100.

Note: OMRON discontinued production of JPt100 Sensors in March of 2003.

Reference Information


Indicated Temperature when Connecting Pt100 Sensor to JPt100 Input

Indicated Temperature when Connecting JPt100 Sensor to Pt100 Input

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Temperature Controllers FAQ