Page top

Primary Contents

Question

What is "Heating and Cooling Control"?

Answer



Temperature control over a controlled object would be difficult if heating was the only type of control available, so cooling control was also added. Two control outputs (one for heating and one for cooling) can be provided by one Temperature Controller.

Heating and Cooling Outputs

Set cooling control (direct operation).

Change the direct/reverse operation setting to direct operation.

For example, if you set the temperature (e.g., to 30 °C), the control output will turn ON when the temperature is above the set temperature and will turn OFF when it's below the set temperature.

If the temperature rises above the set temperature again, the output will turn ON again.

The point at which the output turns ON is also affected by the hysteresis setting.

Applicable Models: All Omron's Temperature Controllers

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Temperature Controllers FAQ