Page top

Primary Contents

Question

Why doesn't the temperature of E5[]N Basic-type Digital Temperature Controllers rise or fall?

Answer



The load is not connected to the correct control output terminals.

Wires are not connected to the correct terminals or load polarity.

There is insufficient contact with the terminals because the terminal screws are loose.

The load power supply is OFF.

The heater has burnt out or deteriorated.

The heat capacity of the heater is insufficient for the load.

The overheating prevention device is not operating.

The reverse/forward operation setting in the Initial Setting Level is incorrect.

The PID constants are not suitable.

The RUN/STOP mode in the Operating Level is set to STOP.

Applicable models: E5CN, E5GN, E5EN, and E5AN

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Temperature Controllers FAQ