Page top

Lead Contents

FAQ00964 of Rotary Encoders FAQ

FAQ No. FAQ00964

Primary Contents

Question

Can regular lead wire be added in the middle of E69-DF[] Extension Cables when it is connected to E6[][] Absolute Encoders and H8P[] Cam Positionesr?

Answer



Trouble will occur in the sense that the rated specifications will not be met. To reduce the effects of noise, use a special E69-DF[] Extension Cable. Do not relay the cable using a terminal block. Doing so will cause the signal to be easily affected by other signal lines.

Applicable model combinations:
E6CP-AG5C-C/H8PS
E6C3-AG5C-C/H8PS
E6F-AG5C-C/H8PS
E6F-AB3C-C/H8PR