Page top

Lead Contents

FAQ01345 of Pressure Sensors FAQ

FAQ No. FAQ01345

Primary Contents

Question

What is the procedure for setting the pressure of E8F2 Pressure Sensor manually?

Answer



Manual Setting

Note:Manual setting can be performed if is selected for the pressure setting method in the initial settings.

1.Press to enter the pressure setting mode, and and the set ON point for OUT1 will be alternately displayed.

2.Change the ON point (for OUT1) using and .

3.Press to select the displayed ON point, and and the set OFF point for OUT1 will be alternately displayed.

4.Change the OFF point (for OUT1) using and .

5.Press to select the displayed OFF point, and and the set ON point for OUT2 will be alternately displayed.

6.Change the ON point (for OUT2) using and .

7.Press to select the displayed ON point, and and the set OFF point for OUT2 will be alternately displayed.

8.Change the OFF point (for OUT2) using and .

9.Press to select the displayed OFF point, and and the set ON point for OUT1 will be alternately displayed.

Returning to Measurement Mode

Saving the set value: Press for approx. 2 s. (Valid for any set value display.)

Not saving the set value: Press and at the same time. (Valid for any set value display.)