Page top

Primary Contents

Question

What is a direct opening mechanism (forcibly opened contacts) ?

Answer



A direct opening mechanism is one that forces open a welded contact by the direct force applied by the actuator (operating section) pressing down.
Safety components with direct opening mechanism (forcibly opened contacts) display the mark(*) on their labels.

Direct Opening Mechanism (Forcibly Opened Contacts)

After the contacts have been forced open, the contacts have enough insulation between them to clear the stipulated impulse withstand voltage (EN 60947-5-1) when the specified operating force (corresponding to DOF) or stroke (corresponding to DOT) is applied against a force of 10 N applied to the contacts (equivalent to the contact weld force).

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Emergency Stop Switches FAQ