![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How can I replace the LED lamp for A22E Emergency Stop Switch with LED illumination?
Answer
Replacing the LED lamp from the Socket Unit
Remove the lock lever and separate the Operation Unit and the Socket Unit. Grip the LED lamp with your fingers, and then rotate the lamp while pressing it into the Socket Unit.
Follow steps 1 and 2 below.
1. Separating the Operation Unit and Socket Unit.
Move the lever in the direction indicated by the arrow in the following figure, and then pull the Operation Unit or the Socket Unit. The lever has a hole with an inside diameter of 6.5 mm, so the lever can be moved in the specified direction by inserting a screwdriver into the hole and then moving the screwdriver.
2. Grip the LED lamp with your fingers, and then rotate the LED lamp while pressing it into the Socket Unit.
Replacing the LED Lamp from the Panel Surface
Using the Tightening Wrench (A22Z-3905), separate the cap from the Operation Unit. Use the Lamp Extractor (A22Z-3901) to replace the LED lamp.
Follow the steps 1 and 2 below.
1. Insert the protrusion of the Tightening Wrench (A22Z-3905) into the cap slot and then turn to remove the cap.
2. Installing the LED Lamp
Insert the Lamp Extractor (A22Z-3901) into the lamp, and then rotate the Extractor while pressing in.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.