![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What are the restrictions when soldering A165E series Emergency Stop Switches?
Answer
There are the following restrictions.
1.Hand soldering: Use a 30-W soldering iron and complete soldering within 5 seconds.
2.Automatic soldering: Use dip soldering at 240°C and solder within 3 seconds.
3.Wait for one minute after soldering before exerting any external force on the solder.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.