![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why can't a Programmable Controller or Programmable Terminal be used for the safety circuit?
Answer
The IEC 60204-1 (JIS B 9960-1) standard specifies that a safety circuit cannot be made using a programmable controller alone. This comes from the general requirement of the same standard that safety related functions must be constructed from proven circuit technology and parts. If the circuit relies on the operation of programmable electronic devices, this requirement may not be satisfied.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.