Page top

Primary Contents

Question

How do I replace the LED for Lighted A165E Emergency Stop Switch?

Answer



Replace the LED by separating the operation unit and the socket unit with A16Z-5080 Socket Unit lamp Extractor. Refer to the following steps 1 to 3 for the replacement procedure.

1.Removing the Socket Unit

Insert A16Z-5080 Extractor into the case guide slot shown in figure below and pull the socket unit straight out while pinching it with the Extractor.

2.Mounting the LED

The following figure shows the mounting direction. Insert the LED so that the protrusions on the LED line up with the narrow guides on the socket unit.

3.Mounting the Socket

Mount the socket unit into the operation unit. There is a specific direction for assembling the operation unit and the socket unit. Assemble the two together with the circle mark on the operation unit aligned with the L engraved in the case guide slot and press until you hear a clicking sound. Also make sure there is no lifting or other problems.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Emergency Stop Switches FAQ