![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Is the color of the Emergency Stop Switch regulated?
Answer
The color is regulated by EN 418, ISO 13850, and JIS 9703. A push button switch that is used for emergency situations must be red, and the background must be yellow.
Reference:
OMRON also provides emergency stop switches integrated with a control boxes. (A22E Series only.) The colors are as given above. A yellow control box is integrated with an emergency stop switch, a legend plate for EMERGENCY STOP, and a connector cable. This Switch complies with IP65 degree of protection.
External View
| Contact structure | Model |
| SPST-NC | A22E-M-01B |
| SPST-NC/SPST-NO | A22E-M-11B |
| DPST-NC | A22E-M-02B |
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.