Page top

Lead Contents

FAQ03426 of Pressure Sensors FAQ

FAQ No. FAQ03426

Primary Contents

Question

How is pressure indicated for E8Y Pressure Sensors?

Answer



The indication method slightly differs between E8Y-A1 and E8Y-A2/A5.

E8Y-A1:
Indicated as 000 Pa to 999 Pa below 1 kPa and, but changes to 1.00-kPa display above 1 kPa.

E8Y-A2/A5:
Indicated as 0.00 kPa to 2.00 kPa or 5.00 kPa whether above or below 1 kPa. Indication is not given in units of 1 Pa.