Page top

Lead Contents

FAQ02059 of General Purpose Relays FAQ

FAQ No. FAQ02059

Primary Contents


The Relay does not operate even when voltage is applied. Why is this?


The following causes are probable.

1.Disconnected Coil

Ultrasonic cleaning or applying an overvoltage may cause the coil to become disconnected.

2.Insufficient Coil Voltage

Check the voltage being applied to the coil. The Relay will not operate if the voltage is lower than the must-operate voltage.

3.Incorrect Polarity of Applied Voltage

A Relay equipped with a diode that absorbs coil counter-electromotive force will not operate properly if the positive and negative voltages applied to the coil are connected incorrectly.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ