Page top

Lead Contents

FAQ02104 of General Purpose Relays FAQ

FAQ No. FAQ02104

Primary Contents

Question

What is the "maximum switching current"?

Answer



It's the maximum current that can be switched by the contacts. Relays cannot be used if this value is exceeded.

Example of the Switching Section (Contacts) Specifications

LoadResistance loadInductive load
(cos Φ = 0.4, L/R = 7 ms)
Rated load220 VAC 5 A
24 VDC 5 A
220 VAC 2 A
24 VDC 2 A
Rated carry current5 A
Maximum switching voltage250 VAC, 125 VDC
Maximum switching current5 A
Contact formDPDT
Contact structureSingle
Contact materialAg

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ