Page top

Lead Contents

FAQ02761 of General Purpose Relays FAQ

FAQ No. FAQ02761

Primary Contents

Question

What should I be aware of when operating MY4 General-purpose Relays AC100V Relay from a distance?

Answer



The distance depends on the type and installation conditions of the cable. Wiring power supplies over a long distance in parallel with power lines may cause reset failure due to voltage generated at both sides of the Relays from float capacitance in the wires when the coil input power supplies are OFF. If reset failure occurs, connect bleeder resistors to both sides of the coil.

Reference Information

Guideline for Cable Length Limits

TypeRelay coil
AC Relays
PreconditionsMust-operate voltage of up to 90% of rated voltage allowed
Calculation of
cable length
Symbols
Formulas

(Formula is applicable up to a cable length of 3 km.)
Example: For MY4 Relays100 VAC, 60 Hz, MY4 with CW Cable

Answer: Value exceeds 3,000 m so there is no problem with cables up to 3 km.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ