Page top

Lead Contents

FAQ02762 of General Purpose Relays FAQ

FAQ No. FAQ02762

Primary Contents

Question

Is the rated current of the contacts for MY2 General-purpose Relays 10 A as written on the Relays or 5 A as written in the datasheet?

Answer



The rated current is 5 A.

The "10 A 250 VAC" written on the Relays is the UL/CSA rating and not the product specification. International ratings of this kind are based on under conditions specified for each standard. They are not the same as the ratings that satisfy conditions, such as the operating ambient temperature, outlined in the datasheet.

Do not use the Relays with currents exceeding 5 A.

Example: The UL standards specify 6,000 operations as the minimum test condition, whereas MY2 specifies 500,000 operations minimum.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ