Page top

Lead Contents

FAQ02763 of General Purpose Relays FAQ

FAQ No. FAQ02763

Primary Contents

Question

How do you find the maximum switching capacity?

Answer



This following graph can be used to find how much current can be applied to the contacts. A description of how to interpret the graph to find out how much current can be applied at what load circuit voltage (contact voltage) is provided below.

The following figure shows how to find the maximum switching capacity for a 200-VAC inductive load.

1.Draw a vertical line where the contact voltage is 200 V (red line).

2.Draw a horizontal line from the point of intersection with the AC inductive load curve (green line).

3.Where the green line intersects the contact current axis is the maximum switching capacity. In this case, the switching capacity is 0.9 A.

Example:

To what voltage must the contact voltage be limited in order to switch a 0.5-A DC inductive load?

Answer:

Keep the voltage below 50 VDC (blue line).

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ