Question
Is the bounce time included in the operating time and the release time?
Answer
No, bounce time is not included in operating time and release time.
The operating time is the time from when current is applied to the coil, until the NO contacts (make contacts) turn ON.
The release time is the time from when the coil is turned OFF, until the NO contacts turn OFF. For double-pole contacts, it is the time until the NC contacts close.
Best-selling, general-purpose relays that can be selected based on operating environment and application
Power-switching Compact General-purpose Relays
Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.