Question
What does the “D2” in MY[]N-D2 General-purpose Relays indicate?
Answer
When transistors are used to operate relays, any effects on the transistor caused by the surge, such as deterioration and breakdown, will be eliminated.
Note:
1.Make sure that the polarity is correct.
2.The reset time will be longer, but it will still be within 20 ms.
3.Diode characteristics:
Reverse breakdown voltage: 1,000 V
Forward current: 1 A
Best-selling, general-purpose relays that can be selected based on operating environment and application
Power-switching Compact General-purpose Relays
Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.