Page top

Lead Contents

FAQ02783 of General Purpose Relays FAQ

FAQ No. FAQ02783

Primary Contents


When twin contact points and cross-bar twin contact points are compared to a single contact point, what are the characteristics of the former?


In minimum load applications, contact reliability of twin contact points is higher than that of a single contact point.

Since twin contact points have simply two contact parts, their failure rate related to contact failure is lower than that of a single contact point.

Additionally, cross-bar twin contact points provide further enhanced contact reliability in minimum load applications thanks to their contact form.

However, this theory is not applied for high power load applications, so that a single contact point without AU plating is adopted.

Contact reliability in minimum load applications

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ