Page top

Lead Contents

FAQ02790 of General Purpose Relays FAQ

FAQ No. FAQ02790

Primary Contents

Question

What is the value in parentheses for models with the coil voltage listed as "100/(110) VAC"?

Answer



"100/(110) VAC" indicates that the coil has 3 ratings.

3 ratings

100 VAC at 50 Hz

100 VAC at 60 Hz

110 VAC at 60 Hz

If the specification has "100/110 VAC," the coil has 4 ratings, i.e., it also has "110 VAC at 50 Hz" in addition to the above. The MY and LY General-purpose Relays are examples of Relays with 4 ratings.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ