Page top

Lead Contents

FAQ02799 of General Purpose Relays FAQ

FAQ No. FAQ02799

Primary Contents

Question

What bleeder resistance is required when operating the AC coil of MY General-purpose Relays from a distance?

Answer



Refer to the following table.

(Typical Values)

Bleeder Resistance for MY4 AC100/110V

Float capacitance (μF)Resistance (kΩ)Wattage (W)
0.05 max.Not required.-
0.05 to 0.1572
0.15 to 0.1762.5
0.17 to 0.1953
0.19 to 0.2344
0.23 to 0.3035
0.30 to 0.4228
0.42 min.115

Bleeder Resistance for MY4 AC200/220V

Float capacitance (μF)Resistance (kΩ)Wattage (W)
0.01 max.Not required.-
0.01 to 0.1288
0.12 to 0.1479
0.14 to 0.15610
0.15 to 0.18512
0.18 min.415

Note:

1.CVV cable: Nominal conductor cross-section: 2 mm2 (7 conductors), Float capacitance between wires: 0.15 to 0.25 (μF/km).

2.The resistance wattages are reference values. Be sure to check the values in the circuit actually used.

Recommended Products

MY

New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays

LY

Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ