Page top

Lead Contents

FAQ02810 of General Purpose Relays FAQ

FAQ No. FAQ02810

Primary Contents


How can we consider the contact resistance in the minimum load area?


When switching a minimum load, contact resistance of the contact points may be considered a problem.

However, even if a high contact resistance happens to be generated, it may recover in the subsequent operation. Also, formation of contact films may increase the contact resistance.

Whether or not a contact resistance value is considered a problem should be judged by the type of problem occurred in the used circuit.

For this reason, a criterion for failure of Relay contact resistance is defined with an initial value. The minimum applicable load is one of the measures of failure and the failure rate is usually expressed as P-level (reference value).

In addition, some of Relay contacts are suitable for minimum load switching and some are not.

Recommended Products


New Latching Levers for Circuit Checking Added to Our Best-selling MY General-purpose Relays


Power-switching Compact General-purpose Relays

G3PE (Three-phase)

Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.

Other General Purpose Relays FAQ