Question
What is the operating voltage of MY2 AC200/220V General-purpose Relays?
Answer
The rated coil voltage is less than 80% of the operating voltage.
Therefore MY2 AC200/220V operates at 200 VAC x 80% = 160 VAC max. (when coil temperature is 23°C).
Best-selling, general-purpose relays that can be selected based on operating environment and application
Power-switching Compact General-purpose Relays
Compact, Slim-profile SSRs with Heat Sinks. Solid State Contactors for Three-phase Heaters Reduced Installation Work with DIN Track Mounting.