![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why is the operating value for the overload factor of motors and relays given as "115% of the current setting value"?
Answer
The JEM 1357 standard for Motors and Relays states that the operating value for the overload factor of static protective relays for motors must be in the range of 105% to 125% of the current setting value.
The operating value of OMRON products is 115% of the current setting value, with a ± 10% setting tolerance for the overload factor. This combines to give a range of 105% to 125%, which satisfies the above standard.
Applicable models: K2CM, SE Motor Protective Relay