Page top

Primary Contents

Question

Which terminals should the G3PX Power Controller inputs be connected to?

Answer



It depends on the type of input.

1. Analog Inputs

(1) 4 to 20-mA or 1 to 5-V Inputs


Terminals: 4 and 5

Note:The terminals are the same (4 and 5) for both current and voltage inputs.

Input impedance: 250 Ω

(2) Analog Inputs Using External Main Setting

2. ON/OFF Pulse Inputs

Terminal numbers 3 to 5

(1) Power ON/OFF Pulse Signal Inputs

Example

(2) Contact ON/OFF Pulse Signal Inputs

Note:There is only one input of whatever kind. The G3PX may be damaged if there is more than one signal is input.

Recommended Products

MY

Versatile and Function-filled Miniature Power Relay for Sequence Control and Power Switching Applications

LY

A Miniature Power Relay

G7Z

Multi-pole Power Relay for Contactor Current Range Capable of Carrying and Switching 40 A at 440 VAC

Other Power Controllers FAQ