Page top

Lead Contents

FAQ01975 of Push Buttons / Indicator Lamps FAQ

FAQ No. FAQ01975

Primary Contents

Question

What can be the cause and what are the possible countermeasures if the M2BJ-B[][] pushbuttons AC/DC shared buzzer does not sound?

Answer



There is a smoothing capacitor in the internal circuit and it is possible that inrush current has caused the switching power supply to overload, resulting in no outputs.

Possible Countermeasures

1.If there is a switching power supply overload, it is possible to reduce the inrush current by connecting an external limiting resistor (20 to 30 Ω) in series.

2.The M2BJ-B[][]-D for DC only has no inrush current.

Recommended Products

61F-G[]N

Improved Design for a More Lightweight Construction and Reduced Standby Power Consumption.

Z

Best-selling Basic Switch Boasting High Precision and Wide Variety

WL, WLM

Wide Range of Two-circuit Switches; Select One for the Operating Environment/Application

Other Push Buttons / Indicator Lamps FAQ