![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the minimum load current value that can be set?
Answer
The load current is limited to 1A at 100% output.
TRIAC or Thyristor output elements have a minimum holding current. If the load current is less than 1A, decrease in output signals cannot make output elements keep in the ON state, so that oscillating waveform may occur or they may not be turned ON.