Page top

Primary Contents

Question

Can multiple Programmable Controllers (PLC) be connected to a single Programmable Terminal (PT)?

Answer




With the Programmable Terminal "NT Series", multiple PLCs cannot be directly connected to a single PT.

In the NT link (1:N mode), PLC:PT=1:N (N= 1 and above), not PT:PLC=1:N.

Only single PLC can be connected to the PT.

In order to collect data of multiple PLCs into a single PLC, link their data through the Controller Link Network to gather information into a single PLC and make the PLC containing gathered information communicate with a PT.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ