![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What method is used to store the screens in the NT30, NT31, NT620, and NT631 Programmable Terminals?
Answer
Screen data is stored in flash memory, so there is no battery backup.
The following data is retained by the battery:
Numeral memory table and character string memory table data in the Programmable Terminal
Display history and alarm history data
Calendar/clock settings
The Battery life expectancy is about 5 years at 25°C.
A C500-BAT08 Lithium Battery is used to back up this data.
The service life will be shorter when the Programmable Terminal is used at higher temperatures.
Replace the Battery as required based on the conditions in which the Programmable Terminal is being used.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.