Page top

Primary Contents

Question

What is the baud rate of high-speed 1:N NT Link communications? Also, how can I switch communications from the standard NT Link protocol?

Answer



The high-speed NT Link's baud rate is 115 kbps.

To set the high-speed NT Link, select the 1:N NT Link protocol in the Programmable Controller Setup and set the baud rate to 115 kbps.

Communications must be set to high-speed 1:N NT Link in the Programmable Terminal as well. Set the communications method in the Programmable Terminal's System Menu.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ