Page top

Primary Contents

Question

In the NS-series Programmable Terminals, is there a way to create a group of buttons so that all of the other buttons go OFF when one of the buttons is ON (i.e., only 1 button can be ON at a time)?

Answer




These buttons, also known as radio buttons, can be created by specifying the same group number to the buttons on the group Tab Page (an Expansion Tab) of the ON/OFF Button Properties Dialog Box. Actually, the radio buttons can be created by setting the desired buttons' action to Alternate, and unifying all of the buttons into the same group on the group Tab Page, which is displayed when the Expansion Tabs are being displayed.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Terminals FAQ