![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How can I import I/O comments that were created with the CX-Programmer FA Integrated Tool Package into the NT-ZJCMX1-EV4 NT Support Tool?
Answer
Use the following procedure to import CX-Programmer I/O into the NT Support Tool.
Steps Prior to Reading I/O Comments:
1.In the CX-Programmer, open the ladder program containing the I/O comments that you want to read. Select File - Save As and save the program in the CXT file format.
2.Click the Window's Start Button in the lower-left corner of the screen, open the folder containing the CX-Programmer Program folder, and select the File Conversion Utility to start the utility. (The utility may be in a different folder if another folder was specified during installation.)
4.Specify a file name and save the file as a text file. The I/O comments will be written to the specified text file as tab-delimited text.
Steps in the NT Support Tool:
1.In the NT Support Tool, select Tools - Import I/O Comments.
2.Set the file type to CX-PIO Comments (Tab Delimited) (*.txt) or All Files (*.*), select the I/O comment file (tab-delimited text file) that was created in step 4 above, and click the OK Button. The I/O comments will be imported.
Note:Windows is a registered trademark of the Microsoft Corporation.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.